Click this button and remove the selected multipath tap.
Indicating the tap index.
Click the check box to enable or disable a specific tap.
Range: 0–100
Default: 1
Enter the delay offset of the tap to the line-of-sight signal.
Range: -40dB to 0 dB
Default: -10
Enter the power offset of the tap to the line-of-sight signal.
Range: -125 kHz to 125 kHz
Default: 5
Enter the Doppler shift of the tap to the line-of-sight signal.